Hi,
It is possible to customize the fields in beacons(I am working with kw41z). I looked into ibeacon and it has an array of 25 bytes. In my case, i want to send one more additional value from my program as a part of 25 bytes.
Is it possible to do that? I tried to modify the code base and all the functions are constant. They expect a static value whereas my new value is dynamic and it changes every second. Can you please tell me if my approach is possible? Any alternatives would also be helpful.
Basically I should be able to witness UUID, Major value along with my dynamically generated value when I scan for the device in my mobile app.
Regards
Niranjan
已解决! 转到解答。
Hello,
How many bytes will you be needing in your packet? If you can provide more details about this I can investigate further on this. I believe it should be possible if the packet you want to send it's compliant with the advertisement packet structure.
Which version of the SDK are you using ? Could you please help me confirm that you are using the latest one available in the SDK builder?
The process to follow will change in case you have a previous version of the examples
Regards,
Estephania
Hello,
if you are exactly looking for a beacon you can check this post https://community.nxp.com/docs/DOC-329201.
Could you please check it and let me know if that it's helpful for you?
Regards,
Estephania
Hi,
Yes, I looked into the document. But the examples/demo applications in SDK shows the advertising fields like UUID,beacon identifier, company identifier are getting added to adData1 as static values which remains unique.
In my application, I want to add a dynamic value like acceleration of device(x or y or z) along with advertising packet. [That is the value has to be added in run time of application rather than during compile time]
Is it possible to add this functionality?
Thanks and Regards
Niranjan
Hello,
How many bytes will you be needing in your packet? If you can provide more details about this I can investigate further on this. I believe it should be possible if the packet you want to send it's compliant with the advertisement packet structure.
Which version of the SDK are you using ? Could you please help me confirm that you are using the latest one available in the SDK builder?
The process to follow will change in case you have a previous version of the examples
Regards,
Estephania
Hi,
Yes, I am able to figure it out and advertise customized packets now. Now I have two new questions
1. How would I restart the beacon advertising every second (beacon application fields A,B,C is getting changed in my project). Any documentation for this? please note that I am not having two tasks in my rtos code. Inside the single main_task I am executing all.
2. The FXOS8700Q is subjected to soft and hard iron magnetic effects(I read this in a community post). But I dont intend to calibrate the device every-time I switch it on. Is there any static offsets to be given? To be specific I want my device to function like an ecompass in android phone.
Thank you for your help.
Thanks and Regards
Niranjan
'Hello,
There is not a specific document to achieve what you are looking for. It won't be possible to do it in the main task, you will need to use a timer and either a task or function triggered to update the values.
About the e-compass, could you please check this post ?
https://community.nxp.com/thread/350457
Regards
Estephania
Hi,
I am able to achieve my task partially. I used NVIC_SystemReset(), but this would reset the entire program. I am looking for reset functionality like pressing SW3 of frdm kw41z would do. (like a reflashing but erasing existing memory). Can you help me in this aspect?
Regards
Niranjan
Hello,
Due to my current load of work, and as this it's a different matter, could you please help me posting it in a different thread ? So we can have the information in a more organized way and also for this to be check not only by me but for other persons as well that might be able to help you
Regards,
Estephania