Customer Evaluation Tool for JN5179

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Customer Evaluation Tool for JN5179

716 Views
prashanthtandel
Contributor I

Hi,

We are using JN5179 as Zigbee Coordinator for our Product. We have designed a High Power module by taking the reference design of JN5179 M16 Module of DK5 and made few changes in DIO to configure the SKYWORKS chip.

We are facing issues while executing Customer Evaluation Tool (JN-AN-1210 - JN517x Customer Module Evaluation Tool). Various readings like RSSI is observed properly on M16 module while the same tests give wrong RSSI results on our production module.

We assume, these issues might be due to changes in DIOs made for our design as shown below.

*** Following are the changes made in our design which are different than the M16 DK5 design.

=================================================================

  1. RFRX (CRX) (DIO0 ---> DIO2) ====> (M16 had DIO0 while our module has DIO2).
  2. RFTX (CTX) (DIO1 ---> DIO3) ====> (M16 had DIO1 while our module has DIO3).
  3. ANT_SEL (DIO4 ---> DIO1) ====> (M16 had DIO4 while our module has DIO1).
  4. CSD Set to HIGH
  5. CHL Set to HIGH
  6. We are using RX LNA mode and TX High Power Mode.

=================================================================

If DIO change is the issue then can you please provide the customer evaluation tool with above changes.

0 Kudos
Reply
1 Reply

529 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

The JN5179 it's not supported for mass market, could you please contact your sales representative for more information about this product? 

Also, please consider that the support is limited for the JN5179. 

Best Regards, 

Estephania

0 Kudos
Reply