Cannot capture packets through Ubiqua

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot capture packets through Ubiqua

828 Views
yuboli
Contributor II

Hello,I have a JN5169USBdongle bought on the official website, I can use it to capture the package;

I have 5169 modules, so I want to make a few JN5169dongle, I burned the JN-SW-4168's own JefficSniffer firmware into the JN5169 module.

1552633536(1).png

Why can't I use Ubiqua to perform packet capture analysis on ZigBee?

1552632979(1).png

The application you selected is not supported by the firmware running on this devece,  why ?

Any one can help ? 
Thanks in advance .

0 Kudos
3 Replies

705 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Daniel,

Could you please try to program the JN devices using the next path?

C:\NXP\bstudio_nxp\sdk\JN-SW-4168\Tools\JennicSniffer\JennicSniffer_JN5169_1000000.bin

B. Installing a Packet Sniffer

Regards,

Mario

0 Kudos

705 Views
yuboli
Contributor II

Thank you!

I downloaded it according to your path, but I still can't.

pastedImage_1.png

pastedImage_2.png

My JN5169 module,as shown below

pastedImage_3.png

What is the reason for this?

0 Kudos

705 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Daniel,

When you program the JN5169, you are in programming mode, the DO0 is in high, isn't it?

After that, the DO0 should be floating before the reset, with this the program will jump to the sniffer code.

Regards,

Mario

0 Kudos