Hi,
I would like to know about the zigbee modules. I want to send the text message using a zigbee to a LED display boards. I have a number of displays to show a different text. Suppose I have a total 50 led display boards, and I used a JN5178x zigbee module for few led boards and for other boards can I used a digi inter modules or silicon lab module. Is it possible to include a different zigbee modules in our network which is created by using a NXP stack. Can you suggest how to get started with the zigbee, which module is best fitted for my requirement, I have a custom board LPC1788.
warm regards
Depends on your application. JN5179, is newer so I will recommend this one.
As alternative for JN, you can also check KW41 that have 512KB Flash, 128 RAM and could works in BLE and 802.15.4 (ZigBee, Thread) in the same time (dual-application supported).
Regards,
Ovidiu
Hi Mohammad,
Considering Zigbee 3.0 or ZigBee Home Automation specification, the interoperability between vendors is subject of certification. So definitely these will work together if the stack is certified.
Below is a link to our website for ZigBee3.0 and ZigBee Home automation application notes:
- ZigBee 3.0|NXP or
- ZigBee Home Automation|NXP .
Considering the topic of your application (Lighting) , you can use JN-AN-1189-ZigBee-HA-Demo application note as a startup.
Regards,
Ovidiu
Thanks Ovidiu,
I look for the new evaluation board JN5169 EK004 and JN5179 SDK, I didn;t find the bit rate of zigbee module, number of channels supported and price. I have a requirement of 250Kbps bit rate, 16 channels. Can you please help me to get that details.
warm regards
Hi Mohammad,
The JN5179 is newer but has limited support. Anyway, we provide different examples compatibles with the JN5169.
As you know the JN517x DK005 is in end of life status. But the module is available.
And the JN5169 is in active status. module and dev kit.
Mario