Hi,
I am working on IW416, and found following problem.
As WIFI client,
How can I receive multicast packets in promisc mode?
Here is some information.
insmod /lib/modules/mlan.ko
insmod /lib/modules/moal.ko cfg80211_wext=0xf fw_name=sdiouartiw416_combo_v0.bin cal_data_cfg=none
# mlanutl mlan0 version
Version string received: SDIW416---16.92.21.p11.2-MM5X16283.p2-GPL-(FP92)
Thanks,
Ethan
解決済! 解決策の投稿を見る。
Hello @EthanHP_Tsai,
Looking internally, the FP92 doesn't support the promisc mode.
Sorry for the inconvenience this may cause you.
BR,
Alexis Andalon
Hello @EthanHP_Tsai,
Could you share the command used to enable the monitor mode?
BR,
Alexis Andalon
Hi Alexis,
First, I use tcpdump to capture packet on mlan0, and I can't see any mDNS packet. When tcpdump start, mlan0 enter to promisc mode.
Then I try to write a simple socket program to bind udp port 5353 and 224.0.0.251, and mDNS packets are received. If I perform the command "ifconfig mlan0 promisc", can't see any mDNS packets.
I think I should be able to receive all packets when promisc mode is set.
Thanks,
Ethan
Hello @EthanHP_Tsai,
Looking internally, the FP92 doesn't support the promisc mode.
Sorry for the inconvenience this may cause you.
BR,
Alexis Andalon
Hi Alexis,
Thanks for your clarification.
Ethan