I have a commercial device containing a JN5169. I can program it, but can't read it, although no read protection is set.
I always chalked this up to some kind of read protection. However, now I purchased some 'empty modules', and these behave exactly the same. Why?
The read fails at 0x200.
I am using these devices now:
Buy Products Online from China Wholesalers at Aliexpress.com
I can flash them, but then it appears like stale data in the EEPROM is messing things up. However, I can't read them or erase the EEPROM.
When using the production flash programmer to erase the eepromp, either full or pdm, i get:
Error erasing EEPROM: Read error loading extension binary into RAM
Just flashing them without verifying works, and the output I get then, is the output I wrote into the application for it, so it is running the new version of software then.
However, when I'm trying to program and verify:
Error: Read error reading Flash at address 0x00000200
I'm using the production flash programmer build 1365. I have also tried flashing from Beyondstudio, this works, but also gives the verification error.
The deviceconfig:
JTAG_ENABLE,VBO_200,CRP_LEVEL0,EXTERNAL_FLASH_NOT_ENCRYPTED,EXTERNAL_FLASH_LOAD_ENABLE
All userdate fields are set to 0xFF.
I see the link to the device contains my order id.
Here's a clean link:
Sorry I misread. I have 6 of YOUR chips lying around here, on boards from different manufacturers, and they all do this. Please don't hide behind the fact it's not one of your boards, it IS one of your chips.
Is there a hardware way to make it read protected?