Can’t build JN-AN-1244

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can’t build JN-AN-1244

624 Views
mariuszjakubows
Contributor I

Hi,

I try to build JN-AN-1244 Dimmable Light under MCUXpresso IDE. First, I had a problem with the SDK path, which seems to be fixed now; however, when the build process starts it’s getting stuck at 20%  and doesn’t move a bit. In the task manager, I see that ZPSConfig is working intensely but I have no clue what can be the problem.

mariuszjakubows_0-1622934648426.png

Mariusz

0 Kudos
Reply
1 Reply

606 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Please click the button 'detail' and make the screenshots. I want to check it. And what mcu you use?

xx.PNG

When it stuck, does the build console goes on showing something?

Does your tool chain installed completely?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply