BeyondStudio for NXP中导入新工程出现错误

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BeyondStudio for NXP中导入新工程出现错误

94,888 Views
2433841893
Contributor I

你好,我开发zigbee项目需要用到JN5169,在按照JN-UG-3098文档中的说明先安装BeyondStudio for NXP再安装JN-SW-4168,之后在安装zigbee Plug-ins的过程中会出错,已截图。忽略这个问题继续安装,完成后,导入JN-AN-1189工程后,在代码中会出现很多错误,已截图,请问是不是还需要下载什么插件吗?

0 Kudos
17 Replies

93,852 Views
ggq
Contributor I

Thank you very much, installed JN516x IEEE 802.15.4 SDK (JN-SW-4163), the above problem is solved, but there are many problems in the source file after Build.

pastedImage_1.png

0 Kudos

93,853 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

The errors you are seeing is Eclipse not being able to resolve various variables and functions within the SDK. You can delete that errors, Look that he Console Path and try to compile again, only see the process in the console section.

Mario

0 Kudos

93,852 Views
ggq
Contributor I

同样问题,导入JN-AN-1174例程编译,出现路径错误。重装好几遍,问题依旧。基于WIN7系统,和操作系统应该无关吧?请指点

pastedImage_1.png

0 Kudos

93,852 Views
2433841893
Contributor I

你好,你在开发工具的安装过程中有没有出现这样的问题,已截图

0 Kudos

93,853 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gao Lei,

I'm sorry. Could you please provide the version that you are working on?

Also, could you please provide step by step the installation process that you did?

Mario

0 Kudos

93,852 Views
2433841893
Contributor I

HI,

All versions are as follows: BeyondStudio for NXP, JN-SW-4141 BeyondStudio for NXP v1308. JN-SW-4163 IEEE802.15.4 SDK v1416. JN-SW-4168 ZigBee-HA-LL v1620

The order of the pictures indicates the steps of the installation. All are behind the default, no changes have been made.

Does anyone else have this problem?

Does your software have any restrictions in China?

0 Kudos

93,852 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gao, 

Could you please try to install the ZigBee Pro with the JN-SW-4170?

Zigbee Pro Plug-In - file:/C:/NXP/bstudio_nxp/sdk/JN-SW-4170/Tools/Eclipse_plugins/com.nxp.sdk.update_site/

Regards,

Mario

0 Kudos

93,852 Views
2433841893
Contributor I

Hi,Mario

This problem also occurs when installing the JN-SW-4170.

Have you reproduced this question?

Is there anyone else in China who has discovered this problem?

0 Kudos

93,852 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gao,

You are working on the JN-AN-1174, aren't you?

You need the JN-SW-4141 and the SDK JN-SW-4163. and you have compilation issue, but if you look the console log, is the compilation process success?

Have you reproduced this question?

No, I am trying to reproduce. I want to understand your application and the process that you are following.

Mario

0 Kudos

93,852 Views
2433841893
Contributor I

How to modify to change the compiled chip model, for example, compile the generated .bin file from JN5169 to JN5168。

0 Kudos

93,852 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gao Lei,

Please look at the next community post.

https://community.nxp.com/thread/480152 

Regards,

Mario

0 Kudos

93,852 Views
2433841893
Contributor I

No, I am working on the JN-AN-1189, There is no problem during the compilation process,and the bin file has been generated. But the file of this project is too big, you can help me recommend an official routine, it is best to use wireless data transceiver interface.

0 Kudos

93,851 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Did you install the JN516x IEEE 802.15.4 SDK (JN-SW-4163)?

IEEE® 802.15.4 for JN516x and JN517x

Regards,

Mario

0 Kudos

93,852 Views
2433841893
Contributor I

Reinstall the JN516x IEEE 802.15.4 SDK according to your method, and a new error has occurred.

0 Kudos

93,852 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gao Lei,

Please look at the next community post. 

https://community.nxp.com/docs/DOC-340028 

Mario

0 Kudos

93,852 Views
2433841893
Contributor I

Hi,Mario Ignacio Castaneda Lopez  Thank you for your answer. There is really no problem during the compilation process,and the bin file has been generated. But there are a lot of errors in source file (.c). Can you help me solve it?

0 Kudos

93,851 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gao Lei,

Open a source file (.c) or a header file (.h),  you will notice that the IDE shows a lot of errors even though the project has not been compiled yet.

The errors you are seeing is Eclipse not being able to resolve various variables and functions within the SDK.

I recommend just looking at the console path.

Mario

0 Kudos