你好,我开发zigbee项目需要用到JN5169,在按照JN-UG-3098文档中的说明先安装BeyondStudio for NXP再安装JN-SW-4168,之后在安装zigbee Plug-ins的过程中会出错,已截图。忽略这个问题继续安装,完成后,导入JN-AN-1189工程后,在代码中会出现很多错误,已截图,请问是不是还需要下载什么插件吗?
Thank you very much, installed JN516x IEEE 802.15.4 SDK (JN-SW-4163), the above problem is solved, but there are many problems in the source file after Build.
Hi,
The errors you are seeing is Eclipse not being able to resolve various variables and functions within the SDK. You can delete that errors, Look that he Console Path and try to compile again, only see the process in the console section.
Mario
同样问题,导入JN-AN-1174例程编译,出现路径错误。重装好几遍,问题依旧。基于WIN7系统,和操作系统应该无关吧?请指点
Hi Gao Lei,
I'm sorry. Could you please provide the version that you are working on?
Also, could you please provide step by step the installation process that you did?
Mario
HI,
All versions are as follows: BeyondStudio for NXP, JN-SW-4141 BeyondStudio for NXP v1308. JN-SW-4163 IEEE802.15.4 SDK v1416. JN-SW-4168 ZigBee-HA-LL v1620
The order of the pictures indicates the steps of the installation. All are behind the default, no changes have been made.
Does anyone else have this problem?
Does your software have any restrictions in China?
Hi Gao,
Could you please try to install the ZigBee Pro with the JN-SW-4170?
Zigbee Pro Plug-In - file:/C:/NXP/bstudio_nxp/sdk/JN-SW-4170/Tools/Eclipse_plugins/com.nxp.sdk.update_site/
Regards,
Mario
Hi,Mario
This problem also occurs when installing the JN-SW-4170.
Have you reproduced this question?
Is there anyone else in China who has discovered this problem?
Hi Gao,
You are working on the JN-AN-1174, aren't you?
You need the JN-SW-4141 and the SDK JN-SW-4163. and you have compilation issue, but if you look the console log, is the compilation process success?
Have you reproduced this question?
No, I am trying to reproduce. I want to understand your application and the process that you are following.
Mario
How to modify to change the compiled chip model, for example, compile the generated .bin file from JN5169 to JN5168。
Hi Gao Lei,
Please look at the next community post.
https://community.nxp.com/thread/480152
Regards,
Mario
No, I am working on the JN-AN-1189, There is no problem during the compilation process,and the bin file has been generated. But the file of this project is too big, you can help me recommend an official routine, it is best to use wireless data transceiver interface.
Hi,
Did you install the JN516x IEEE 802.15.4 SDK (JN-SW-4163)?
Regards,
Mario
Hi,Mario Ignacio Castaneda Lopez Thank you for your answer. There is really no problem during the compilation process,and the bin file has been generated. But there are a lot of errors in source file (.c). Can you help me solve it?
Hi Gao Lei,
Open a source file (.c) or a header file (.h), you will notice that the IDE shows a lot of errors even though the project has not been compiled yet.
The errors you are seeing is Eclipse not being able to resolve various variables and functions within the SDK.
I recommend just looking at the console path.
Mario