Hi,
I am looking for a BT5.0 transceiver which can help to transmit and receive the voice and music.
I already have a host IC with codec, but, just need a BT5.0 transceiver to transmit and receive the voice and music signal from the other device.
So, can KW35 or QN908x fulfill my requirement?
Arm® Cortex®-M0+|Kinetis® KW35Z/36Z Bluetooth Low Energy 32-bit MCUs | NXP
QN908x: Ultra-Low-Power Bluetooth Low Energy System on Chip (SoC) Solution | NXP
BR
Matthew
Hello,
The Bluetooth LE does not have a profile for audio, nonetheless, you might be able to use the GFSK and create your own frame like the Bluetooth LE and adapt it to send audio through the radio as it has a 2M PHY in the QN9080 case.
Still, if you are looking for an audio solution, have you checked this device ?
Regards,
Estephania