BGU8052

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BGU8052

542 Views
869019315
Contributor I

Can BGU8052 be used at 1.2ghz?How does 0IP3 and Gain change?

Tags (1)
0 Kudos
Reply
1 Reply

485 Views
LPP
NXP Employee
NXP Employee

Please refer to this application note:
https://www.nxp.com/docs/en/application-note/AN11902.pdf

It provides the measurement results that have been carried out on the standard 1900MHz BGU8052 evaluation boards at 1.3GHz.


The measured IP3O is 35dBm. This value fits the datasheet spec (IP3O>32dBm) at 1900MH. We do not expect noticeable difference at 1.2GHz.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply