Hi,
I am using M2-JODY-W377 module and want to set the TX power in the tx_countinuous mode.
used these commands:
echo "rf_test_mode=1" >> /proc/mwlan/adapter0/config
echo "band=1" >> /proc/mwlan/adapter0/config
echo "channel=128" >> /proc/mwlan/adapter0/config
echo "bw=4" >> /proc/mwlan/adapter0/config
echo "tx_power=10 2 2" >> /proc/mwlan/adapter0/config
echo "tx_continuous=1 1 0xAAA 0 3 7" >> /proc/mwlan/adapter0/config
but it seems, module doesn't start to transmit(can't see anything on spectrum analyzer).
if I don't set the "tx_power", it start to transmit but it doesn't stop with 'echo "tx_continuous=0" >> /proc/mwlan/adapter0/config' command.
Another question: In UM11490 document it is mentioned that "The commands(tx_power) only set power if caldata is already loaded in the firmware", But it isn't explained HOW? What is this caldata?
Hi @shaun_wu,
Thanks for your reply. I also changed the bandwidth but still same results. when I use the following set of commands
~# modprobe moal mod_para=nxp/wifi_mod_para.conf
~# echo "rf_test_mode=1" >> /proc/mwlan/adapter0/config
~# echo "band=1" >> /proc/mwlan/adapter0/config
~# echo "channel=128" >> /proc/mwlan/adapter0/config
~# echo "bw=0" >> /proc/mwlan/adapter0/config
~# echo "tx_continuous=1 1 0xAAA 0 3 7" >> /proc/mwlan/adapter0/config
it starts to transmit but doesn't stop by
~# echo "tx_continuous=0" >> /proc/mwlan/adapter0/config
And by using the below set of commands, it even doesn't start to transmit.
~# echo "rf_test_mode=1" >> /proc/mwlan/adapter0/config
~# echo "band=1" >> /proc/mwlan/adapter0/config
~# echo "channel=128" >> /proc/mwlan/adapter0/config
~# echo "bw=0" >> /proc/mwlan/adapter0/config
~# echo "tx_power=10 0 2" >> /proc/mwlan/adapter0/config
~# echo "tx_continuous=1 1 0xAAA 0 3 7" >> /proc/mwlan/adapter0/config
~# echo "tx_continuous=0" >> /proc/mwlan/adapter0/config
I also tried different parameter values for "tx_power", but nothing changed.
Here are the output messages of the driver.
[ 191.410174] mlan: loading out-of-tree module taints kernel.
[ 191.488541] wlan: Loading MWLAN driver
[ 191.492676] wlan: Driver loaded successfully
[ 191.492742] wlan: Register to Bus Driver...
[ 191.501376] wlan_pcie 0000:01:00.0: enabling device (0000 -> 0002)
[ 191.507647] Attach moal handle ops, card interface type: 0x206
[ 191.516593] PCIE9098: init module param from usr cfg
[ 191.521615] card_type: PCIE9098, config block: 0
[ 191.526247] cfg80211_wext=0xf
[ 191.529213] max_vir_bss=1
[ 191.531847] cal_data_cfg=none
[ 191.534841] mac_addr=00:50:43:20:12:34
[ 191.538605] fw_name=nxp/pcieuart9098_combo_v1.bin
[ 191.543317] txpwrlimit_cfg=nxp/txpower_DE.bin
[ 191.547700] rx_work=1 cpu_num=4
[ 191.550868] Attach mlan adapter operations.card_type is 0x206.
[ 191.558000] Request firmware: nxp/pcieuart9098_combo_v1.bin
[ 192.149434] FW download over, size 620880 bytes
[ 193.666012] WLAN FW is active
[ 193.668984] on_time is 193607003595
[ 193.672492] Download txpwrlimit_cfg=nxp/txpower_DE.bin
[ 193.702222] fw_cap_info=0x81c3fa3, dev_cap_mask=0xffffffff
[ 193.707760] max_p2p_conn = 8, max_sta_conn = 64
[ 193.726792] wlan: version = PCIE9098--17.92.5.p11-MM5X17283.p2-GPL-(FP92)
[ 193.734596] wlan_pcie 0000:01:00.1: enabling device (0000 -> 0002)
[ 193.740890] Attach moal handle ops, card interface type: 0x206
[ 193.747616] PCIE9098: init module param from usr cfg
[ 193.752679] card_type: PCIE9098, config block: 1
[ 193.757377] cfg80211_wext=0xf
[ 193.760377] max_vir_bss=1
[ 193.763068] cal_data_cfg=none
[ 193.769911] mac_addr=00:50:43:20:52:56
[ 193.773758] fw_name=nxp/pcieuart9098_combo_v1.bin
[ 193.778515] txpwrlimit_cfg=nxp/txpower_DE.bin
[ 193.782940] rx_work=1 cpu_num=4
[ 193.786133] Attach mlan adapter operations.card_type is 0x206.
[ 193.802091] Request firmware: nxp/pcieuart9098_combo_v1.bin
[ 193.808335] WLAN FW already running! Skip FW download
[ 193.813438] WLAN FW is active
[ 193.816462] on_time is 193754473516
[ 193.820002] Download txpwrlimit_cfg=nxp/txpower_DE.bin
[ 193.835859] fw_cap_info=0x81c3fa3, dev_cap_mask=0xffffffff
[ 193.841400] max_p2p_conn = 8, max_sta_conn = 64
[ 193.861533] wlan: version = PCIE9098--17.92.5.p11-MM5X17283.p2-GPL-(FP92)
[ 193.869024] wlan: Register to Bus Driver Done
[ 200.512779] Sleep confirm command failed
[ 200.518036] Sleep confirm command failed
Regards,
Javad
Hi @shaun_wu,
I use a Started Kit with i.MX8 as processor and runs Yocto Linux. And also use M2-JODY-W377 which is connected to the starter kit through PCI.
Firmware: pcieuart9098_combo_v1.bin
Driver Version: PCIE9098--17.92.5.p11-MM5X17283.p2-GPL-(FP92)
card_type: PCIE9098
Regards
Javad
Hi everyone,
I am facing a similar problem using the test modes exposed via proc-fs (under "/proc/mwlan/adapter0/config").
I am using an iMX8 based platform with a custom Yocto based Linux.
Tuning the radio to 20MHz channels works without an issue, but using higher bandwidths doesn't work at all.
$ cat /proc/mwlan/adapter0/config
hardware_status=0
netlink_num=31
drv_mode=7
hssetpara=7,0xff,200,400
rf_test_mode=1
tx_antenna=1
rx_antenna=1
band=1
bw=4
channel=36
radio_mode[0]=1
radio_mode[1]=9
total rx pkt count=0
rx multicast/broadcast pkt count=0
rx fcs error pkt count=0
tx_power=
tx_continuous=0
tx_frame=1 110 0xaaa 256 1 20 0 0 0 0 0 0 0 -1 -1 -1 -1 -1 -1 -1 00:00:00:00:00:00
he_tb_tx=0
trigger_frame=0
I tried all sorts of different channel / bw / mcs_rate combinations (e.g. using channel 42, which is a defined 80MHz), but never got more than 20MHz out of the 88W9098.
We are currently on PCIE9098--17.68.1.p136.32-MXM5X17366.p16-GPL-(FP68)(R38).
Best regards