88mw320 CRC mismatch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

88mw320 CRC mismatch

1,293 次查看
youngsoo
Contributor I

I built the matter lighting app on Ubuntu 20.04 LTS by referring to the github below.

https://github.com/NXP/matter/tree/v1.0.0.2-tag-nxp/examples/lighting-app/nxp/mw320

 

There was a problem with libusb, so I moved the bin file to Windows and wrote it using both J-Link commander and J-Flash lite.

boot2 0x1F00 0000 / mcufw 0x1F01 0000 / wififw 0x1F35 0000

After writing firmware, the following problem occurred.

__________________________________________________

<< MW320 MCU firmware: [lighting-app] >>
version: [2.9.11-001]
[0.002]CHIP:-:  init mw320 sdk
CRC mismatch[psm] Warn: scan: Invalid obj (b2e4) at the end of data area off: 0 addr: A58
[0.211]CHIP:-: [PSM]: (start, len)=(0xa58, 0xf828)

__________________________________________________

Is there any way to solve this problem?
Should I use the generated flashprog.py?

标签 (1)
0 项奖励
回复
6 回复数

1,261 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I'm going to try to replicate this on my side.

I'll let you know my findings.

Regards,

Daniel.

0 项奖励
回复

1,224 次查看
youngsoo
Contributor I

Hi Daniel.

I think it can be a reference, so I attach the binary file and py file that I have built.

 

Regards,

Bae.

0 项奖励
回复

1,200 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Thank you for sharing the files.

I was able to flash the example with the files you shared with me using Ubuntu and flashprog. The only difference is that I used the OpenOCD and flashprog that came with the WMSKDA V6.0.r7.p3 bundle.

ubuntu@ubuntu1804:~/Desktop/wmsdka/wmsdka_bundle-V6.0.r7.p3$ ./sdk/tools/OpenOCD/flashprog.py -l ./mw320_sdk_copy/layout-4m.txt --boot2 ./mw320_sdk_copy/boot2.bin --wififw ./mw320_sdk_copy/mw32x_uapsta_W14.88.36.p172.bin --mcufw ./mw320_sdk_copy/chip-mw320-lighting-app.mcufw.bin

Example Running:

<< MW320 MCU firmware: [lighting-app] >>
version: [2.9.11-001]
[0.002]CHIP:-:  init mw320 sdk
[0.199]CHIP:-: [PSM]: (start, len)=(0x330000, 0x10000)
[7.101]CHIP:-:  mw320 init complete!

Could you please verify OpenOCD is correctly installed in your PC or try to flash it in the same way as me?

Regards,

Daniel.

0 项奖励
回复

1,185 次查看
youngsoo
Contributor I

Thank Daniel.

 

I'm currently having issues with libusb on Ubuntu 20.04 LTS.

Downloading to use the VM. Or I'm going to test it on my MacBook.

  

Q.

Is there a difference between how to use flashprog.py and openOCD and how to use j-link commander or J-Flash Lite?

 

Regards,

Bae.

0 项奖励
回复

1,112 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I'm sorry for the late response.

I was also able to flash the app using J-Link Commander.

I believe you might be missing to load the MCUFW, Wi-Fi FW and layout as a flash image. E.g. layout-4m.bin, not layout-4m.txt.

You can create your own flash partitions using the mw_img_conv.py file.

Please follow my steps in a command line:

 

1. Create your layout flash image: python mw_img_conv.py layout layout-4m.txt layout-4m.bin

2. Create a Wi-Fi FW flash image: python mw_img_conv.py wififw mw32x_uapsta_W14.88.36.p173.bin mw32x_uapsta_W14.88.36.p173.fw.bin

3. In J-Link commander flash the layout binary: loadbin <file_path>\layout-4m.bin 0x1F004000

4. Flash the Wi-Fi FW: loadbin <file_path>\mw32x_uapsta_W14.88.36.p172.fw.bin 0x1F350000

5. Flash the MCUFW: loadbin <file_path>\chip-mw320-lighting-app.mcufw.bin 0x1F010000

6. Reset the MW320

 

You should be able to run the example.

I hope this helps,

Daniel.

0 项奖励
回复

1,085 次查看
youngsoo
Contributor I

It is solved. thank Daniel.

0 项奖励
回复