Hello,
We are trying to interface the 88W89997 in usb mode for both wifi and bt part. From the documentation I see that i can use an USB 2.0 Interface. Is this stament true? For the driver part, is there any guide to follow?
Thanks in advance
Hello @mhammouda ,
>>Is this stament true?
Yes, it it.
http://www.azurewave.com/wireless-modules-nxp.html
AW-CM276NF LGA model can be configured as USB2.0/3.0,PCIe,SDIO interface.
>>For the driver part, is there any guide to follow?
you can follow these steps to get mass market driver and firmware
--driver
#git clone http://source.codeaurora.org/external/imx/mwifiex.git
#cd mwifiex
#git tag
#git checkout lf-5.10.72_2.2.0
--firmware
https://github.com/NXP/imx-firmware/tree/lf-5.10.72_2.2.0/nxp
If you want to get more documents or materials, you will have to sign NDA with NXP.
you only need to submit a case from our website for NDA, my colleague will help you sign it.
Have a good day!
Regards,
weidong