Where do I find the Vybrid manufacturing tool? Can it operate via USB0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where do I find the Vybrid manufacturing tool? Can it operate via USB0?

1,423 Views
markwatson
Contributor III

We have been programming the internal boot select fuses via the debug port, but would like to find an easier method.  Can the Vybrid Manufacturing tool support this and can it operate using USB0?

Labels (1)
0 Kudos
Reply
2 Replies

1,264 Views
art
NXP Employee
NXP Employee

The Vybrid MFGtool software can be downloaded from here (check the "Programmers" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/vfxxx-controller/f-series...

It is meant to operate on the USB0 port. It can be used to program the OTP bits, refer to the documentation included.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,264 Views
markwatson
Contributor III

To be more specific, we need to program the OCOTP to force the system to boot from the SD card.  It seems that the Manufacturing tool should be able to download a small program to blow the fuses, but it is unclear how to accomplish this.

Thanks.

0 Kudos
Reply