Where do I find the Vybrid manufacturing tool? Can it operate via USB0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where do I find the Vybrid manufacturing tool? Can it operate via USB0?

829件の閲覧回数
markwatson
Contributor III

We have been programming the internal boot select fuses via the debug port, but would like to find an easier method.  Can the Vybrid Manufacturing tool support this and can it operate using USB0?

ラベル(1)
0 件の賞賛
2 返答(返信)

670件の閲覧回数
art
NXP Employee
NXP Employee

The Vybrid MFGtool software can be downloaded from here (check the "Programmers" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/vfxxx-controller/f-series...

It is meant to operate on the USB0 port. It can be used to program the OTP bits, refer to the documentation included.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

670件の閲覧回数
markwatson
Contributor III

To be more specific, we need to program the OCOTP to force the system to boot from the SD card.  It seems that the Manufacturing tool should be able to download a small program to blow the fuses, but it is unclear how to accomplish this.

Thanks.

0 件の賞賛