Vybrid VF610 instability at 500Mhz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid VF610 instability at 500Mhz

615件の閲覧回数
HeMyFAE
NXP Employee
NXP Employee

We are looking at running our VF610s at 500 MHz and are running into some issues.  The custome have applied the 5))MHz patches that are ontop of u-boot 2013.07, provided by Timesys, against u-boot 2015.07 and see instability after 5 hours. Is there a patchset from NXP that also handle e6235 ( ANADIG: Unstable clock if PFD_FRAC divisor is 19)?

Is Timesys Uboot the latest to support 500Mhz or do we have more updated one?

Regards,

hy

ラベル(1)
0 件の賞賛
1 返信

424件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid we do not provide Linux BSP for Vybrid, assuming third party (Timesys) for it.

Regards,

Yuri.

0 件の賞賛