Vybrid M4 DDR icf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid M4 DDR icf

1,018 Views
kubiznak_petr
Contributor V

Hi,

where is it possible to get an IAR linker file (icf) for MQX operation under M4 and DDR memory? Currently in MQX 4.0.2 there is only INT RAM configuration for M4. There is a DDR configuration for A5 though. Is there any reason why not to use DDR memory from the M4 core? My application, which needs to run on M4, is getting too large and does not fit into the internal ram (at least not with the current ram.icf file).

Labels (2)
Tags (6)
0 Kudos
5 Replies

512 Views
juangutierrez
NXP Employee
NXP Employee

Hi

Well I can find there is one at

Program Files\IAR Systems\Embedded Workbench 6.5\arm\examples\Freescale\VF6xx\128MB_ddr_m4.icf

However, I needed to modify it in order to get successfully running the GettingStarted project from M4 and DDR .

For running the GettingStarted sample:

1) open the project:

Program Files\IAR Systems\Embedded Workbench 6.5\arm\examples\Freescale\VF6xx\TWR-VF600\build\iar\projects\getting_started\GettingStarted.ewp

2) Select the build option for M4 Debug DDR

Besides the name this runs from SRAM

3) Point to the linker file attached

    Project -> Options -> Linker -> Linker configuration file -> Override default

          Populate the field with the path to the attached icf file

4) Rebuild and Dowload the image

   This time you can check that it is indeed running from DDR.

This is bare-metal code but I think you can base on this for whatever change needed for MQX.

512 Views
kubiznak_petr
Contributor V

Bit later but still, I tested your icf file on the GettingStarted demo (thank you again), with negative result though - it failed to validate the downloaded code (see attached debug log).

To save your time - I do not personally need it anymore, so do not push on it. On the other hand, there might be some general need for M4 DDR configuration...

0 Kudos

512 Views
jbs
Contributor II

I may run into the same issue soon. Did you find a solution, or any additional information?

0 Kudos

512 Views
kubiznak_petr
Contributor V

Hi jbs,

I did not manage to solve the M4 DDR issue, the available icf files simply did not work for me. I found a pretty elegant workaround though. Suppose you do not run MQX on the A5 core, intram memory area reserved for that configuration (0x3F050000 - 0x3F07FEFF, i.e. 191.75k) can be appended to M4 memory space. Use _mem_extend() call to do that. Just make sure A5 does not use the memory (e.g. Linux suits to this condition).

0 Kudos

512 Views
kubiznak_petr
Contributor V

Hi Juan,

thank you for your reply, it seams to be very helpful. I knew about this file but as it didn't work, I ignored it. I'll get back to your post in the next week and will reply as soon as I evaluate it.

Petr

0 Kudos