Hi,
I am quite new to the community and to the Freescale (NXP) boards in general, so hope my question is not too trivial.
We are using DS-5 v5.20.1, TWR-VF65GS10 and want to use A5 core with MQX4.2. Hovewer, we also want to use Processor Expert.
This discussion Processor Expert and MQX support for Vybrid mentions that "one thing you could do to migrate the PE code to MQX is just add the PE definitions in the BSP so MQX can support the code and drivers generated by PE" and that "the best way to get PEx to work with MQX is to add PEx to an existing MQX project... Details on how to do this is already documented in one of the PEx guides." I was unable to find that guide or any other information/explanation of these methods.
Was anyone able to get this working?
Any help will be greatly appreciated!
Regards,
Klim
已解决! 转到解答。