Hi community.
Our customer has below questions.
· What is the SDRAM density upper limit of Vybrid?
Also, please tell me if there is a restriction.
- Would you Please reference layout connect to SDRAM and Vybrid.
- Attached is an excerpt of the iMX6 dual circuits.
I wired it the same as?
- Please tell me the way if i want to use two by switching the DDR SDRAM.
Best Regards.
解決済! 解決策の投稿を見る。
Hello Takashi-san,
main DRAM memory space is mapped from 0x8000_0000 to 0xFFFF_FFFF. (2GB)
It can be used directly by Cortex-A5 only. Cortex-M4 has PPB from 0xE000_0000.
Cortex_M4 can address from 0x8000_0000 to 0xDFFF_FFFF. (1.5GB)
Cortex_M4 also can use alias from 0x0080_0000-0x0FFF_FFFF to eliminate wait state (248MB)
Maximal address space is no. of CS x 2^Address x no.banks x datapathwidth
= 1 x 2^ (11 COLs + 16 ROWs) x 8 x 2 = 1 x 128MB x 8 x 2 = 2GB for 16 bit interface
= 1 x 2^ (11 COLs + 16 ROWs) x 8 x 1 = 1 x 128MB x 8 x 1 = 1GB for 8 bit interface
On reference platform are used only signals col 0-9, row 0-12 -> 1 x 2^23 x 8 x 2 = 128MB (1Gb) (K4B1G1646G-BCF8).
In this case we use range 0x8000_0000 to 0x87FF_FFFF
/Jiri
Hi Takashi -san,
Vybrid supports a maximum of 1 GB of SDRAM.
It has a 16-bit wide data bus, so we recommend to use a single 16-bit device for easy layout.
Please refer to the hardware developers guide for layout information. You can re-use the DDR layout of the tower or EVB boards.
These boards have a DDR layout that does not require termination resistors and we have correct DDR controller configuration for this layout.
You can find the hardware develpers guyde and more information at:
VF6xx MPUs with ARM Cortex-A5/M4 Core|Vybrid|NXP
Best regards,
Richard
Hi Richard.
Thank you for your reply.
I read VYBRID RM of section 3.7.2.1. DDR maximum address space.
There are described on " As a result, the maximum accessible memory area is 1Gbyte(125MBit).
But , On the other , in Table4-1 are described on allow 2GB accessible below.
-------------------------------------------------------------------------------------------------------------------------------------------------
Table 4-1. Device Memory Map
CM4 Address Range Size CM4 Alias System Address (A5) Region Description
[Start Addr - End [MB] [Start Addr - End
Addr] Addr]
----------------------------------------------------------------------------------------------------------------------------------------------------
0x8000_0000-0xdfff_ffff 1536 0x8000_0000-0xdfff_ffff DDR
0xe000_0000-0xffff_ffff 512 N/A Reserved CM4 Private Periphera Bus (PPB 512 N/A 0xe000_0000-0xffff_ffff DDR (A5 only)
-------------------------------------------------------------------------------------------------------------------------------------------------------
Question.
Table 4-1 of Device memory map has been described on 0x8000_0000 ~ 0xdfff_ffff, 0xE000_0000 ~ 0xffff_ffff (A5 only),
Since the maximum 1Gbit only available,It is the memory 0x8000_0000 ~ 0xbfff_ffff that can be used.
Is it correct?
Thanks,
Best.
T.Takahashi
Hello Takashi-san,
main DRAM memory space is mapped from 0x8000_0000 to 0xFFFF_FFFF. (2GB)
It can be used directly by Cortex-A5 only. Cortex-M4 has PPB from 0xE000_0000.
Cortex_M4 can address from 0x8000_0000 to 0xDFFF_FFFF. (1.5GB)
Cortex_M4 also can use alias from 0x0080_0000-0x0FFF_FFFF to eliminate wait state (248MB)
Maximal address space is no. of CS x 2^Address x no.banks x datapathwidth
= 1 x 2^ (11 COLs + 16 ROWs) x 8 x 2 = 1 x 128MB x 8 x 2 = 2GB for 16 bit interface
= 1 x 2^ (11 COLs + 16 ROWs) x 8 x 1 = 1 x 128MB x 8 x 1 = 1GB for 8 bit interface
On reference platform are used only signals col 0-9, row 0-12 -> 1 x 2^23 x 8 x 2 = 128MB (1Gb) (K4B1G1646G-BCF8).
In this case we use range 0x8000_0000 to 0x87FF_FFFF
/Jiri