Does the VYBRID (MVF61NS151CMK50) support DDR3L running at 1.35V?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the VYBRID (MVF61NS151CMK50) support DDR3L running at 1.35V?

ソリューションへジャンプ
481件の閲覧回数
kevindarrah
Contributor I

I want to use this part (MT41K64M16TW-107)

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
339件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Kevin,

Theoretically speaking, if the only difference from the regular DDR3 is the power rail voltage, then the Vybrid SDRAM controller, capable of working at 1.2V and 1.5V, works at any value inside this range. And the DDR_REF (logic threshold) is defined externally - at the level of 1/2 of the actual power rail value. So, the answer at the first glance is "yes".

At the same time, the Vybrid datasheet does not contain any detailed data for this power voltage value due to that it has not been validated for it. Based on the common industry practice, if a requirement for a new use-case comes from the field and triggers additional validation effort on our side, it has to first be approved by the Marketing team based on the prospective sales numbers to those interested in this use-case, etc.

Without that, unfortunately, a user will have to run this mode on his own risk.

sincerely, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
1 返信
340件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Kevin,

Theoretically speaking, if the only difference from the regular DDR3 is the power rail voltage, then the Vybrid SDRAM controller, capable of working at 1.2V and 1.5V, works at any value inside this range. And the DDR_REF (logic threshold) is defined externally - at the level of 1/2 of the actual power rail value. So, the answer at the first glance is "yes".

At the same time, the Vybrid datasheet does not contain any detailed data for this power voltage value due to that it has not been validated for it. Based on the common industry practice, if a requirement for a new use-case comes from the field and triggers additional validation effort on our side, it has to first be approved by the Marketing team based on the prospective sales numbers to those interested in this use-case, etc.

Without that, unfortunately, a user will have to run this mode on his own risk.

sincerely, Naoum Gitnik.

0 件の賞賛