DSTREAM not able to connect to custom vybrid board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSTREAM not able to connect to custom vybrid board

Jump to solution
1,155 Views
abdulnihad
Contributor III

When I tried to debug application using DS-5 and ARM DSTREAM on custom vybrid platform, it shows

Unable to connect to USB:003604
Failed to read 4 bytes from AP 0 @ 0x40001020 on DAP
Bad argument to command.
Unable to connect to USB:003604.

Can some one tell me what is this error and how can I fix it.

Also When I do auto config in debug hardware configuration tool come with ARM DS-5 bundle, it shows auto config fail.

Even when I try to select platform, there is no vybrid platform available.

0 Kudos
1 Solution
626 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Abdul,

please check if the problem occurs also on Tower module.

If problem occurs on Tower module we can help you (we will ask ARM) or you can directly contact ARM (DSTREAM producer)

If problem occurs only on your module, then please check voltage rails, reset circuit and connection of JTAG connector. It could be easy to check it pins are toggling similarly like on tower module.

/Jiri

View solution in original post

0 Kudos
4 Replies
627 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Abdul,

please check if the problem occurs also on Tower module.

If problem occurs on Tower module we can help you (we will ask ARM) or you can directly contact ARM (DSTREAM producer)

If problem occurs only on your module, then please check voltage rails, reset circuit and connection of JTAG connector. It could be easy to check it pins are toggling similarly like on tower module.

/Jiri

0 Kudos
626 Views
abdulnihad
Contributor III

Hi,

Its working now...There was some problem with reset line.

DSTREAM is also work with vybrid tower.

Thanks for your support.

BR/-

Nihad

0 Kudos
626 Views
zixet
Contributor II

I'm facing the same problem and same error. Could you please elaborate how did you fix that?

0 Kudos
626 Views
naoumgitnik
Senior Contributor V

Hello Abdul,

I am not a SW person but before we dig deeper, have you tried to search the other DS-5 and ARM DSTREAM related threads on the Community, please? - In the upper right corner of the page.

Once in a while, there appear "cannot connect" questions here...

Sincerely, Naoum Gitnik.

0 Kudos