Respected Colleagues and Bruno Castelucci
I have made modifications for Phytec Vybrid Cosmic+ Board to the board-pcl052.c file in the way that Bruno Castelucci did in the board-pcm052.c file (Discussion SPI Driver on Linux Side).
Test from the shell like Bruno's with modeprobe spi_mvf_dspi returned:
# modprobe spi_mvf_dspi
DSPI: Coldfire master initialized
#
Does it mean that DSPI is correctly initialized? How can I trace it further? I see that Bruno got bunch of lines as a trace report.
So, can somebody attach a working example code for any SPI chip (EEPROM, FLASH, RTC, etc.) for Vybrid VF61 under Timesys Linux to make test on some real hardware chip.
This will help a lot for further development.
File with DSPI modifications for Phytec Cosmic+ Board is attached.
Thanks in advance.
With best regards,
Dragan Kujovic
Original Attachment has been moved to: board-pcl052.c.txt.zip
解決済! 解決策の投稿を見る。
Respected timesyssupport,
thanks for your suggestions regarding DSPI.
I have made a DSPI example code for the Phytec Vybrid Cosmic+ board under Timesys Linux.
DSPI under Timesys Linux now works like a charm (tested on the real hardware SPI chips). Sample code has all SPI basic settings (SPI Mode, SPI Speed, SPI number of bits per word and LSB/MSB option).
Sample code and configuration files are attached.
With best regards,
Dragan Kujovic
Hello Dragan,
After you load the spi_mvf_dspi module, you should also probe the spidev module. After doing so, you should see /dev/spidevX.Y entries for each spi interface enabled in your Linux board configuration file. For relevant spidev documentation and test source, please see the Documentation/spi/spidev file in your kernel sources:
https://www.kernel.org/doc/Documentation/spi/spidev
Thanks,
Timesys Support
Respected timesyssupport,
thanks for your suggestions regarding DSPI.
I have made a DSPI example code for the Phytec Vybrid Cosmic+ board under Timesys Linux.
DSPI under Timesys Linux now works like a charm (tested on the real hardware SPI chips). Sample code has all SPI basic settings (SPI Mode, SPI Speed, SPI number of bits per word and LSB/MSB option).
Sample code and configuration files are attached.
With best regards,
Dragan Kujovic
timesyssupport can you help to review this case?