Отладка VF6xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Отладка VF6xx

1,190件の閲覧回数
lyudmilavoronin
Contributor II

On board TWRVF65GS10 (MCU) there is K20 JTAG Header. Can I use K20 JTAG Header for programming and debugging of an my own board with the processor Vybrid vf6xx? 

ラベル(1)
5 返答(返信)

884件の閲覧回数
Yuri
NXP Employee
NXP Employee

The following also may be helpful :

Vybrid® VF6xx Tower® System Kit with ARM DS-5|NXP 

Regards,

Yuri.

0 件の賞賛

884件の閲覧回数
lyudmilavoronin
Contributor II

Thanks for references!

I read section 7 (Debug Interfaces) of Hardware Development Guide for Vybrid.
I also watched the electric circuit TWR-VF65SG10_SCH.pdf, on which there is 10 pin JTAG port
(J2,Serial Interface, JTAG K20 header).

On my own board (on the model) there is 10 pin JTAG port too, which is connected
to the Vybrid VF6xxx (Vybrid VF6xxx on my own board too).

On the basis these documents I have come to a conclusion, that
I can connect my own board (model) to JTAG K20 header on TWR-VF65GS10, then
connect USB cable to PC and to TWR-VF65GS10 board, after that I can debug and program my own model.
Is it right or not? It seems to me, that in section 7 it is told not concrete.
I would like to know more precisely, yes or not?

Excuse for my English.
Have a great day too.

0 件の賞賛

884件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  You may look at section 2.4 (Debug interfaces) of TWR-VF65GS10 Tower Module User’s Guide.

 

< http://www.nxp.com/docs/en/user-guide/TWRVF65GS10UG.pdf >

 

  Three (separate) debugging interfaces are provided on the TWR-VF65GS10 module:

• OpenSDA with CMSIS-DAP on Micro-B OTG USB connector J3 ;

• JTAG on header J5 ;

• ARM ETM (Embedded Trace Macrocell) on connector J11.

 

  The first (OpenSDA with CMSIS-DAP firmware) does not require additional

hardware (probe) for (minimal) debugging.

  The second is JTAG approach, that is most powerful, but requires additional

hardware such as DSTREAM of ARM. It allows working in bare metal environment.

 

  For Your board, where there is 10 pin JTAG port, connected to the Vybrid VF6xxx -

the second, JTAG based, approach may be applied. In order to use OpenSDA with CMSIS-DAP on Your board it is necessary to have Kinetis with corresponding firmware (and schematic). If You board is part of Tower system, as the second Vybrid based one - it is possible to rely on existing OpenSDA with CMSIS-DAP,

assuming Your Vybrid code is already working (with help of a JTAG debugger).

Regards,

Yuri.

0 件の賞賛

884件の閲覧回数
lyudmilavoronin
Contributor II

Thank you very much!

I read section 2.4 and assumed that it is necessary to buy the additional

equipment, but wanted to know precisely.

On our board (bare metal) there are no Kinetis with corresponding firmware

(and schematic) and we have to buy the additional

hardware, to start the Vybrid VF6xxx on the our model.

Thanks, I consider a question solved.

2017-07-20 7:12 GMT+03:00 Yuri <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Отладка VF6xx

reply from Yuri Muhin

<https://community.nxp.com/people/Yuri?et=watches.email.thread> in *Vybrid

Processors* - View the full discussion

<https://community.nxp.com/message/925924?commentID=925924&et=watches.email.thread#comment-925924>

884件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to section 7 (Debug Interfaces) of Hardware Development Guide for Vybrid

Family of MCUs, User’s Guide, Rev. 1, 05/2015.

http://www.nxp.com/docs/en/user-guide/VYBRIDHDUG.pdf 

Summary Page :

VF6xx MPUs with ARM Cortex-A5/M4 Core|Vybrid|NXP 

Recommended software and tools :

VF6xx MPUs with ARM Cortex-A5/M4 Core|Vybrid|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛