Where is the tool VIT Text-to-Model?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the tool VIT Text-to-Model?

2,503件の閲覧回数
yugandhar421
Contributor II

Hi,

I want to try the Text to Model tool which is used to generate VIT AI model for custom wake word and custom voice commands. In the video demo available at MCU Tech Minutes: Text-to-Model Demo Using NXP’s Voice Intelligent Library (VIT) on i.MX RT1170 MCUs they are talking about the Text to Model tool, but no link provided from where it can be downloadable.

 

More than 4 hours I searched in Google and NXP website, but no where I can find this tool, all docs only I can see with terms VIT and Text to Model. It is better if NXP people provides the links of software/tools mentioned in the demo, which saves programmers time atleast.

 

If anybody knows about this tool please help me.

 

Thanks,

Yugandhar

0 件の賞賛
3 返答(返信)

2,205件の閲覧回数
nxp79866
NXP Employee
NXP Employee

Hello Yugandhar,

 

The VIT model generation tool is now available online at   https://vit.nxp.com/#/

 

 

Thanks,

Laurent 

 

0 件の賞賛

2,439件の閲覧回数
nxf49874
NXP Employee
NXP Employee

@FelipeGarcia  Is the VIT SDK open? If yes, where can I download it? I checked the SDK V2.10.0 for RT1170, but VIT project is not found.

0 件の賞賛

2,489件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Yugandhar,

The tool is not public that is why is not located in our website. Sorry for the inconvenience.

Best regards,

Felipe

0 件の賞賛