The EdgeLock™ SE050 family provides a root of trust at the IC level. This CC EAL6+ certified secure element also supports compliance to standards such as ISO/IEC 62443 SL3. The EdgeLock SE050 stores the keys and credentials to manage authentication and access rights securely. But how are those credentials stored on the secure element? And what about changing or updating the credentials in a secure way in the field?
Along with a demo consisting of various NXP components you will experience how to provision and change credentials on an EdgeLock SE050 for secure access for industrial and smart home applications. You will also learn about the different options to manage credentials and how to use NXP’s EdgeLock 2GO Managed Service to configure your IoT device. Following the demo we will go through the different HW and SW building blocks and explain how to implement such a use case based on NXP solutions.
NXP components include: EdgeLock SE050 Secure Element, EdgeLock 2GO Service, i.MXRT1060 Crossover MCU, CLRC663 NFC Frontend, 88W8977 WiFi 4 and Bluetooth SoC (using PAN9026 module).
Presenters:
Antje Schütz, Senior Marketing Manager IoT Security, NXP
Massimo Incerti, EMEA Distribution CAS Manager, NXP