Hello
Is it possible to make the NTAG 424 DNA tags "read-only" using the TapLinx SDK for Android?
Thank you.
#ntag424dna
Hello,
NTAG 424 DNA can be configured as Read-Only with help of TapLinx SDK. Please check APPLICATION NOTE - NTAG 424 DNA and NTAG 424 DNA TagTamper features and hints, chapter "6.15 Write to CC - using Cmd.WriteData, CommMode.PLAIN" (link). Two things to do to make the transition into Read-only life-cycle:
* In order to write/change data to CC File, you need to Authenticate before with key 0x00.
Method to use to change access rights:
changeFileSettings(int fileNumber, NTAG424DNAFileSettings fileSettings);
Best regards,
UK