[NTAG424DNA] - Configure tags as read-only

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[NTAG424DNA] - Configure tags as read-only

1,480件の閲覧回数
ukcas
NXP Employee
NXP Employee

Hello


Is it possible to make the NTAG 424 DNA tags "read-only" using the TapLinx SDK for Android?

 

Thank you.

#ntag424dna

ラベル(1)
0 件の賞賛
返信
1 返信

1,479件の閲覧回数
ukcas
NXP Employee
NXP Employee

Hello,


NTAG 424 DNA can be configured as Read-Only with help of TapLinx SDK. Please check APPLICATION NOTE - NTAG 424 DNA and NTAG 424 DNA TagTamper features and hints, chapter "6.15 Write to CC - using Cmd.WriteData, CommMode.PLAIN" (link). Two things to do to make the transition into Read-only life-cycle:

  • Write read-only byte into CC file (E103)*
  • Set WRITE access rights of NDEF file to 0xN (N = number of any key from 0 to 4, so write access for the ones knowing that key) or 0xF (no WRITE access for anyone)

* In order to write/change data to CC File, you need to Authenticate before with key 0x00.


Method to use to change access rights:
changeFileSettings(int fileNumber, NTAG424DNAFileSettings fileSettings);

Best regards,

UK