Updating T4240QDS boot from SDK v1.5 to v1.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Updating T4240QDS boot from SDK v1.5 to v1.8

Jump to solution
1,741 Views
ch6
Contributor I

Hello,

I am attempting to update a T4240QDS from SDK v1.5 to 1.8. However, I would like to leave bank 0 alone and only update bank 4 with the new u-boot.

Here are the changes that were made to the alternate bank (bank 4) from bank 0, using images from SDK v1.8:

- RCW at 0xec000000

- U-boot at 0xebf40000

- Fman ucode at 0xebf00000

- U-boot env at 0xebf20000 (with mods to ubootaddr and fman_ucode env vars to the SDK v1.8 NOR flash memory mapping)

When switching to the alternate bank (either with command "qixis altbank" or changing SW6[1:4] to 0100), the system hangs and there is no debug output to the serial terminal.

Is this the correct way to update to the newer SDK? Or do both banks need to be updated to SDK v1.8 since the NOR flash memory map is different?

Thanks,

Chris

Labels (1)
0 Kudos
1 Solution
1,488 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Chris,

You didn't use the correct u-boot image, you used the u-boot image for secure boot, please use the normal u-boot image u-boot-T4240QDS.bin, I attached it for you.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
1,488 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Chris,

The images deployment addresses should be correct for SDK 1.8.

Do you use T4240 Rev 1.0 or Rev 2.0 board? Did you use the correct RCW image?

Is possible for you to provide the u-boot log(including SDK 1.8 images deployment steps on bank0)?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,488 Views
ch6
Contributor I

Here is the bank 0 u-boot log:

U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 15 2013 - 18:54:15)

CPU0:  T4240E, Version: 2.0, (0x82480020)

Core:  E6500, Version: 2.0, (0x80400120)

Clock Configuration:

        CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,

        CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,

        CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,

        CCB:733.333 MHz,

        DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:183.333 MHz

        FMAN1: 733.333 MHz

        FMAN2: 733.333 MHz

        QMAN: 366.667 MHz

        PME: 533.333 MHz

L1:    D-cache 32 kB enabled

        I-cache 32 kB enabled

Reset Configuration Word (RCW):

        00000000: 16070019 18101916 00000000 00000000

        00000010: 04383060 30548c00 ec020000 f5000000

        00000020: 00000000 ee0000ee 00000000 000307fc

        00000030: 00000000 00000000 00000000 00000028

Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x14, vBank: 0

FPGA: v6 (T4240QDS_2014_0211_1852), build 547 on Wed Feb 12 00:52:40 2014

SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz

I2C:   ready

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM M391B1G73QH0-CMA

Detected UDIMM M391B1G73QH0-CMA

Detected UDIMM M391B1G7EQH0-CMA

22 GiB left unmapped

     DDR: 24 GiB (DDR3, 64-bit, CL=13, ECC on)

        DDR Controller Interleaving Mode: 3-way 4KB

        DDR Chip-Select Interleaving Mode: CS0+CS1

VID: Core voltage 1029 mV

Flash: 128 MiB

L2:    2048 KB enabled

enable l2 for cluster 1 fec60000

enable l2 for cluster 2 feca0000

Corenet Platform Cache: 1536 KB enabled

Using SERDES1 Protocol: 1 (0x1)

Using SERDES2 Protocol: 28 (0x1c)

Using SERDES3 Protocol: 6 (0x6)

Using SERDES4 Protocol: 12 (0xc)

SRIO1: enabled

SRIO2: disabled

NAND:  512 MiB

MMC:  FSL_SDHC: 0

EEPROM: CRC mismatch (137e3224 != 00000000)

PCIe1: Root Complex, no link, regs @ 0xfe240000

PCIe1: Bus 00 - 00

PCIe2: disabled

PCIe3: Root Complex, no link, regs @ 0xfe260000

PCIe3: Bus 01 - 01

PCIe4: disabled

In:    serial

Out:   serial

Err:   serial

Net:   Fman1: Uploading microcode version 106.4.10

Failed to connect

Failed to connect

Fman2: Uploading microcode version 106.4.10

FM1@DTSEC5 [PRIME], FM2@DTSEC5

Hit any key to stop autoboot:  0

=>

0 Kudos
1,489 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Chris,

You didn't use the correct u-boot image, you used the u-boot image for secure boot, please use the normal u-boot image u-boot-T4240QDS.bin, I attached it for you.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,488 Views
ch6
Contributor I

Thank you, Yiping. This worked for running SDK 1.8 on bank 4.

Running "bitbake u-boot" had set the soft-link in deploy/images/t4240qds/ to the one for secure boot.

I assumed this was correct since we want to call esbc_validate from the u-boot command line before burning fuses, but I will open a separate discussion for this.

0 Kudos
1,488 Views
ch6
Contributor I

Hello Yiping,

It is a Rev 2.0 board. On bank 4, the RCW is now using the image titled rcw_1_27_5_11_1666MHz_rev2.bin from the SDK 1.8 ISO.

Bank 0 was left as SDK 1.5 and only bank 4 was updated to SDK 1.8.

When running from bank 4, there is no u-boot log shown upon reset now (after updating that bank to SDK 1.8).

Here are the commands used on bank 0 to update bank 4 (I don't have those logs anymore):

tftp 1000000 u-boot-T4240QDS_SECURE_BOOT.bin

protect off 0xebf40000 +c0000

erase 0xebf40000 +c0000

cp.b 1000000 0xebf40000 +c0000

protect on 0xebf40000 +c0000

tftp 1000000 fsl_fman_ucode_t4240_r2.0_106_4_15.bin

protect off 0xebf00000 +20000

erase 0xebf00000 +20000

cp.b 1000000 0xebf00000 20000

protect on 0xebf00000 +20000

tftp 1000000 rcw_1_27_5_11_1666MHz_rev2.bin

protect off 0xec000000 +20000

erase 0xec000000 +20000

cp.b 1000000 0xec000000 20000

protect on 0xec000000 +20000

I can post the u-boot log for bank 0 shortly, but it is still the default SDK 1.5 image.

Thank you!

Chris

0 Kudos