T4240: boot: For the different FLASH BASE address, botorom can not start up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240: boot: For the different FLASH BASE address, botorom can not start up

496 Views
carlpeng
Contributor II

When NOR flash BA set as 0xff00_0000, and LAW of IFC set as 0xff00_0000, and size set as 16M, bootrom can startup.

but if I set the NOR flash BA and LAW of IFC as 0xf800_0000, and size as 128M, the same bootrom can not startup.

Could you please help to give some suggestions?

Thank you,

Carl

Labels (1)
0 Kudos
1 Reply

357 Views
ufedor
NXP Employee
NXP Employee

Please ensure that the bootrom is programmed into the uppermost physical area of the flash - i.e. at the end of 128MB.

0 Kudos