T2080 with XFI 10G without PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 with XFI 10G without PHY

4,237件の閲覧回数
tapyang
Contributor III

Dear, all:

I am developing the 10GBase-kr network of T2080, and our board designed that the serdes XFI is connected with XFP optical module directly and without use 10G PHY.

I changed the DTS as follows:

fm1mac9: ethernet@e0000 {
phy-connection-type = "xgmii";
fixed-link = <1 1 10000 0 0>;
};

However, It doesn't work. What should I do now?

Looking forward for your reply and thanks!~

ラベル(1)
タグ(1)
6 返答(返信)

3,663件の閲覧回数
tapyang
Contributor III

Hi, Dear bpe:

The FSL_10GBASE_KR on SDK2.0 has already enabled. And, I checked the MDIO_XFI_PCS_SR1[PCS_RX_LNK_STAT] is not up.

When start the kernel, it says as followed:

pastedImage_1.png

what should I do now?

0 件の賞賛
返信

3,663件の閲覧回数
bpe
NXP Employee
NXP Employee

By defining the "fixed-link" property you effectively disable any PHY
initialization. This is the simplest approach which relies on
out-of-reset settings. You can check the link status in
MDIO_XFI_PCS_SR1[PCS_RX_LNK_STAT] and in the similar bit on the far
end. If the link does not go up automatically, consider enabling
FSL_10GBASE_KR option for SDK 2.0 or FSL_BACKPLANE for later kernels
and declaring the PHY in the Device Tree.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,663件の閲覧回数
tapyang
Contributor III

Hi, dear bpe:

Thanks for your reply very much!

I will try it, and thank you again!

Have a nice day,

Yang

0 件の賞賛
返信

3,663件の閲覧回数
tapyang
Contributor III

Hi, All:

I just want to know that how to configure for 10G network without PHY!!!

Thx!

0 件の賞賛
返信

3,663件の閲覧回数
tapyang
Contributor III

Dear, NXP Engineers:

This project is very hurry, and I have tried a lot of methods what I can try.

Please give me some notice for this, thank you!

Yours

0 件の賞賛
返信

3,663件の閲覧回数
tapyang
Contributor III

Hi, Dear:

I think the 10G XFI without PHY need modify the "dtsi" file, and without burn PHY microcode.

Then what about the driver? I have already fixed the SPEED, then what should I do?

Looking forward for your reply!

Thx!

0 件の賞賛
返信