Hi all,
My T2080RDB base custom board is using 0x6D & 0x2D or 0x6C & 0x29 combination of SERDES protocol. With this combination of protocol selection, both SRIO1(SRIO1) and SRIO2(SRIO2) is 4x. Can I config SRIO1(SRIO1) or SRIO2(SRIO2) to 1x and then keep another one to 4x in this SERDES protocol?
Best regards!
River
There is no need for additional configuring, because the link width is determined automatically and it will be 1 if only lane 0 of the SRIO link is connected to the target device.