T1040: chip selects issue in uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1040: chip selects issue in uboot

752件の閲覧回数
gouravjain
Contributor IV

Hi,

I want to enable some more chip selects from IFC controller. Tried to make changes in u-boot also, but its got hanged.

Here are the changes made by me,

1) T104xRDB.h

#define CONFIG_SYS_RAYCOM1_BASE    0xFF900000

#define CONFIG_SYS_RAYCOM1_BASE_PHYS       (0xf00000000ull | CONFIG_SYS_RAYCOM1_BASE)

#define CONFIG_SYS_CSPR3_EXT    (0xf)

#define CONFIG_SYS_CSPR3        (CSPR_PHYS_ADDR(CONFIG_SYS_RAYCOM1_BASE_PHYS) \

                                | CSPR_PORT_SIZE_8 \

                                | CSPR_MSEL_GPCM \

                                | CSPR_V)

#define CONFIG_SYS_AMASK3       IFC_AMASK(64*1024)

#define CONFIG_SYS_CSOR3        0x0

/* RAYCOM1 Timing parameters for IFC CS2 */

#define CONFIG_SYS_CS3_FTIM0            (FTIM0_GPCM_TACSE(0x0e) | \

                                        FTIM0_GPCM_TEADC(0x0e) | \

                                        FTIM0_GPCM_TEAHC(0x0e))

#define CONFIG_SYS_CS3_FTIM1            (FTIM1_GPCM_TACO(0x0e) | \

                                        FTIM1_GPCM_TRAD(0x1f))

#define CONFIG_SYS_CS3_FTIM2            (FTIM2_GPCM_TCS(0x0e) | \

                                        FTIM2_GPCM_TCH(0x0) | \

                                        FTIM2_GPCM_TWP(0x1f))

#define CONFIG_SYS_CS3_FTIM3            0x0

2) tlb.c

#ifdef CONFIG_SYS_RAYCOM1_BASE

        SET_TLB_ENTRY(1, CONFIG_SYS_RAYCOM1_BASE, CONFIG_SYS_RAYCOM1_BASE_PHYS,

                      MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

                      0, 14, BOOKE_PAGESZ_256K, 1),

#endif

3) law.c

#ifdef CONFIG_SYS_RAYCOM1_BASE_PHYS

         SET_LAW(CONFIG_SYS_RAYCOM1_BASE_PHYS, LAW_SIZE_64K, LAW_TRGT_IF_IFC),

#endif

pls let me know where im doing wrong. Any more configuration is required???

--

Gourav

ラベル(1)
0 件の賞賛
3 返答(返信)

460件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Gourav Jain,

What kind of device is configured at IFC CS2? How do you decide IFC Timing parameters for this device?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

460件の閲覧回数
gouravjain
Contributor IV

Hi Yiping,

Issue got resolved. It was there because of IFC clock, which was higher than expected for end device.

thanks for you interest in my post..

--

Gourav

0 件の賞賛

460件の閲覧回数
hareeshp
Contributor II

Hi gourav jain,

   Could you please share what you had tried to solve this issue?. Because we are also facing the same issue.

0 件の賞賛