T1040 Serdes to Phy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1040 Serdes to Phy

639 次查看
gokulkrishnan
Contributor III

Hi,

I was planning on using one of the Serdes of the T1040 chip as 1G to the external world using a Phy. What setting must I put in the phy for it to work properly. Serdes or SGMII. Also is there anything I need to do configure in the chip T1040 ?

Could you elaborate on the Autonegotiation setting too.

Regards 

Gokul.

标签 (1)
0 项奖励
1 回复

356 次查看
alexander_yakov
NXP Employee
NXP Employee

The question is specific to PHY and, therefore, depends on PHY model and vendor.

From the processor side, there is no difference between "Serdes" and "SGMII" in regards to Ethernet PHY connection - if Ethernet PHY is connected to this particular Serdes lane, than this lane is configured to "SGMII" mode.

Please look T1040 Reference Manual, Table 31-1 "Supported SerDes Options" for more details.

0 项奖励