T1024 Single Clock Mode and JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 Single Clock Mode and JTAG

Jump to solution
659 Views
bltuna
Contributor II

I consider using T1024 in single clock mode, however on the T1024RDB Quick Start document, it's written that "In Single Clock mode, JTAG cannot work to connect CPU". Is this a limitation of development board or T1024? If this is valid for both of them, how could I program flash without u-boot in single clock mode?

Thanks,

Tuna

Mentioned Document: https://www.nxp.com/webapp/Download?colCode=T1024RDBQS&location=null&fasp=1&WT_TYPE=Quick%20Referenc... 

Labels (1)
0 Kudos
1 Solution
553 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

This is limitation of the development board only.
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
554 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

This is limitation of the development board only.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos