IFC vxBus-driver for T2080RDB on VxWorks-7 with FSL_T2T4_1.0.9.1 BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IFC vxBus-driver for T2080RDB on VxWorks-7 with FSL_T2T4_1.0.9.1 BSP

616 次查看
rajeshrajeti
Contributor I

Hi *,

I’m working on T2081 with VxWorks 7.0.

I couldn’t find compatible driver for IFC “fsl,ifc” in VxWorks-7.0, but the same is supported in Linux.

The lack of IFC driver is hampering NOR Flash device registration, for which driver already exists: “micron, cfi-flash”.

BSP’s target.ref did mention about not supporting the NOR/NAND flash devices.

  1. So, is there any plan for supporting IFC vxBus-driver in upcoming BSP releases?
  2. Is there any way to make the NOR flash devices work in VxWorks-7.0?

Thanks & Regards,

Rajesh

标签 (1)
0 项奖励
回复
1 回复

422 次查看
alexander_yakov
NXP Employee
NXP Employee

Sorry, there is no support for VxWorks available from NXP, we support only Linux.

For VxWorks-related questions please contact VxWorks vendor - Wind River

 

Wind River 


Have a great day,
Alexander
TIC

0 项奖励
回复