I'm working with vxworks to bring it up on t1042D4RDB board I saw on SDK 1.9 that i need for (T1042 rev 1.1) -fsl_fman_ucode_t1040_r1.1_106_4_15.bin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I'm working with vxworks to bring it up on t1042D4RDB board I saw on SDK 1.9 that i need for (T1042 rev 1.1) -fsl_fman_ucode_t1040_r1.1_106_4_15.bin

625 次查看
michayardeny
Contributor III

where do I get this file fsl_fman_ucode_t1040_r1.1_106_4_15.bin ?

Micha

标签 (1)
0 项奖励
1 回复

448 次查看
ralftruebenbach
Contributor III

You can find the actual version in QorIQ Linux SDK v2.0 (QorIQ Linux SDK v2.0 PPC64E5500 IMAGE.iso/t1040d4rdb-64b/fsl_fman_ucode_t1040_r1.1_*)

There is also a git repo for the fman µcode (including a version overview):

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0