Hi,
I have been working on T1040RDB and the SDK which i have been using is 3.1.
I want to uio_seville driver which works on internal L2 switch of T1040 processor.
Can you please suggest how to compile the driver in SDK 3.1?
解決済! 解決策の投稿を見る。
I compiled your uio-seville source code in Yocto SDK 3.1 build environment, I encountered the attached compilation errors.
Please check your uio-seville source code again.
HI,
I was able to compile and run the seville driver. Thanks a lot for the help
After recompiling Linux Kernel, have you also recompiled uio_seville module at the same time.
yeah did that...even though getting the error
adding to the latest query
I am using rootfile system from SDK 2.0 and linux & uio_seville driver from SDK 3.1