CKSTP_OUT_B actual use on E6500 devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CKSTP_OUT_B actual use on E6500 devices

640 Views
benjaminlux
Contributor I

Hello, 

Regarding the CKSTP_OUT_B output pin of the T2081.

As it appears on E6500RM that "The e6500 core does not take a checkstop, as is the case with some previous e500 cores."

Could you please clarify wether the CKSTP_OUT_B is actually driven on the T2081, if yes could you please detail the associated conditions.

Regards,

BL

Labels (1)
0 Kudos
1 Reply

502 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, e6500 core does not take checkstop.

CKSTP_OUT_B may be only asserted by other hardware (PEX and DMA) fatal/illegal condition.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos