Booting from NOR Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting from NOR Flash

581 次查看
John_K
Contributor I

I am planning on booting from the (T1040) IFC_Bus using NOR Flash. The UM states that "Before fetching the first instruction from the NOR flash, the IFC flash timing registers are loaded with default timing parameters." My question is assuming default timing parameters is the reset setting of the IFC_FTIM0_CSn_NOR register which is reset to all 0's and all 0's is specified as reserved, how am I supposed to determine the timing of the boot accesses from IFC bus during reads after reset.

Thanks.

标签 (1)
0 项奖励
回复
1 回复

417 次查看
Pavel
NXP Employee
NXP Employee

Look at the Table 24-4 of the T1040 Reference Manual Rev 1:

https://www.nxp.com/webapp/Download?colCode=T1040RM&location=null&fasp=1&WT_TYPE=Reference%20Manuals...

 

This Table shows IFC values for NAND and NOR RCW reading and NOR boot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复