What is the difference between DLA-LS-DVLPR-NL and DLA-LS-SPLST-NL license for CodeWarrior Suite?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between DLA-LS-DVLPR-NL and DLA-LS-SPLST-NL license for CodeWarrior Suite?

ソリューションへジャンプ
2,732件の閲覧回数
ts1234
Contributor III

What is the difference between the two different kind of licenses for CodeWarrior Suite?

$2999 Annual License (DLA-LS-DVLPR-NL)
$4999 Annual License (DLA-LS-SPLST-NL)

What are the additional features provided by DLA-LS-SPLST-NL?

Please confirm if u-boot debugging and NAND/NOR flash write feature is available with DLA-LS-DVLPR-NL?

 

 

0 件の賞賛
1 解決策
2,715件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello, 

In the Buy Parametrics tab (second column) here you will see the table containing all the features that the CWA-LS-DVLPR-NL suite has https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

The difference with the CWA-LS-SPLST-NL is that it will share the same features as the Developer suite plus the features below:

  • DDR Validation tool: The DDR (Double Data Rate RAM Memory) Validation tool (DDRv) is a software application that helps you “tune” the DDR settings that can be the most difficult to get "centered."
  • SerDes Validation: The SerDes Validation tool (SerDes-v) is a software application that helps you “tune” the SerDes settings so you can get the optimal SerDes performance.
  • Debug print Ability to perform printf-like operations from for bare-metal, Linux kernel or Linux user-space applications directly in hardware trace buffers. This vastly reduces logging facility intrusiveness.
  • General purpose program Arm® Trace Ability to configure, retrieve and display Arm® core trace including program and data.

 

Best Regards, 

Paulina

元の投稿で解決策を見る

1 返信
2,716件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello, 

In the Buy Parametrics tab (second column) here you will see the table containing all the features that the CWA-LS-DVLPR-NL suite has https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

The difference with the CWA-LS-SPLST-NL is that it will share the same features as the Developer suite plus the features below:

  • DDR Validation tool: The DDR (Double Data Rate RAM Memory) Validation tool (DDRv) is a software application that helps you “tune” the DDR settings that can be the most difficult to get "centered."
  • SerDes Validation: The SerDes Validation tool (SerDes-v) is a software application that helps you “tune” the SerDes settings so you can get the optimal SerDes performance.
  • Debug print Ability to perform printf-like operations from for bare-metal, Linux kernel or Linux user-space applications directly in hardware trace buffers. This vastly reduces logging facility intrusiveness.
  • General purpose program Arm® Trace Ability to configure, retrieve and display Arm® core trace including program and data.

 

Best Regards, 

Paulina