CodeWarrior licensing and limitations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior licensing and limitations

4,242 次查看
lox
Contributor I

What are the differences between the Special Editions/Suites of CodeWarrior and the evaluation versions of CodeWarrior?

 

The license and registration FAQ is a bit vague Licensing and Registration FAQ

>Freescale makes it easy to evaluate products by offering free trial versions that offer all features of the product to use for a specified time period. We also offer Special Editions for key Freescale architectures that offer limited feature tools that are free to use for all Freescale customers.

 

Is the "free to use" in the Special Editions perpetually as long as you comply to the e.g. code size limitations or are they also time limited e.g. 30 days?

 

On this page CodeWarrior Development Tools

the special edition is listed as a "free trial" version. Is that "free trial" perpetually or time limited as well as restricted with e.g. codesize?

 

Is a version of CodeWarrior offered for free perpetually (with or without limitations, not considering evaluations that are time limited)?

 

Thanks!

标签 (1)
2 回复数

1,539 次查看
TICS_Fiona
NXP Employee
NXP Employee

Both Evaluation Edition and Special Edition are free.

Evaluation Edition works same as professional edition, but it has 30-day time restriction.

Special Edition has no time limit, but it has code size and feature restriction. For details, please refer to this document:

http://www.freescale.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

0 项奖励
回复

1,539 次查看
Robinwithu
Senior Contributor I

Hi Lo,

please see this review you will get everything

http://mcuoneclipse.com/2013/05/04/review-of-codewarrior-for-mcu10-4/

Thanks and Regards,

Robin

0 项奖励
回复