can not install an applet into jcop 4 p71 with error "6F00"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can not install an applet into jcop 4 p71 with error "6F00"

498 Views
chenchengbei
Contributor I

I use the tool Pyapdu tool/pyResMan/snooper to install my applet of cap file.

the package of cap file can be downloaded into the cards , but the applet can not be installed with an error "6F00"

APDUs:

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 88 18 13 5D A6 17 90 02 11 04 95 01 34 80 01 88 81 01 10 84 08 80 80 80 80 80 80 80 80 5F 49 41 04 A1 DE D6 E9 BC D6 F1 73 E7 93 36 DC 6E 68 BC 87 0A 9F 28 FD AE 56 99 E6 20 BF 27 25 D7 C1 1F D9 45 47 D2 83 C0 22 D9 98 E6 1C 4A DC 06 ED DC B8 AC 23 11 22 12 FA 22 47 10 36 68 31 2D 61 2D AA
>>6D 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 50 00 00 08 08 9E 72 BB 3B 5F 01 3A 1C
>>00 00 31 15 27 04 48 20 65 68 01 02 02 25 05 F6 5F 04 B9 11 E4 17 92 03 AA 67 F5 E5 90 00

<<84 82 00 00 10 CA 8D 15 52 3D A7 04 B0 E0 D1 6F 11 FD EE 4C E8
>>90 00

<<80 F2 20 00 02 4F 00
>>07 A0 00 00 01 51 53 50 01 00 05 01 02 03 04 05 01 00 06 00 11 22 33 44 55 01 00 06 01 02 03 04 05 01 01 00 07 45 47 59 48 43 57 57 01 00 09 A0 00 00 00 62 03 01 0C 01 01 00 90 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 88 18 13 5D A6 17 90 02 11 04 95 01 34 80 01 88 81 01 10 84 08 80 80 80 80 80 80 80 80 5F 49 41 04 A1 DE D6 E9 BC D6 F1 73 E7 93 36 DC 6E 68 BC 87 0A 9F 28 FD AE 56 99 E6 20 BF 27 25 D7 C1 1F D9 45 47 D2 83 C0 22 D9 98 E6 1C 4A DC 06 ED DC B8 AC 23 11 22 12 FA 22 47 10 36 68 31 2D 61 2D AA
>>6D 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 50 00 00 08 E5 F8 E1 77 2B 28 E2 94 1C
>>00 00 31 15 27 04 48 20 65 68 01 02 02 26 F1 0D 0D 39 C4 AF 4B 8F 3C 7F 6E FC E7 29 90 00

<<84 82 00 00 10 10 8B 0C 0A 68 AD 15 B7 BA 8A 5F F7 6D 0B 0A E8
>>90 00

<<80 F2 40 00 02 4F 00
>>08 01 02 03 04 05 06 07 08 07 00 07 00 11 22 33 44 55 00 07 00 07 01 02 03 04 05 01 00 07 00 0A A0 00 00 00 62 03 01 0C 01 01 07 00 90 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 88 18 13 5D A6 17 90 02 11 04 95 01 34 80 01 88 81 01 10 84 08 80 80 80 80 80 80 80 80 5F 49 41 04 A1 DE D6 E9 BC D6 F1 73 E7 93 36 DC 6E 68 BC 87 0A 9F 28 FD AE 56 99 E6 20 BF 27 25 D7 C1 1F D9 45 47 D2 83 C0 22 D9 98 E6 1C 4A DC 06 ED DC B8 AC 23 11 22 12 FA 22 47 10 36 68 31 2D 61 2D AA
>>6D 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 50 00 00 08 AE 83 E5 07 B5 09 C9 20 1C
>>00 00 31 15 27 04 48 20 65 68 01 02 02 27 DA 5A F4 C6 B1 A7 D2 8D 8E 6D AB 2E 40 61 90 00

<<84 82 00 00 10 20 65 00 55 AC 91 CE E5 D0 14 3B 6A FE EA E1 3E
>>90 00

<<80 E6 0C 00 20 07 45 47 59 48 43 57 57 08 45 47 59 48 43 57 57 00 08 45 47 59 48 43 57 57 00 01 00 02 C9 00 00
>>6F 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 88 18 13 5D A6 17 90 02 11 04 95 01 34 80 01 88 81 01 10 84 08 80 80 80 80 80 80 80 80 5F 49 41 04 A1 DE D6 E9 BC D6 F1 73 E7 93 36 DC 6E 68 BC 87 0A 9F 28 FD AE 56 99 E6 20 BF 27 25 D7 C1 1F D9 45 47 D2 83 C0 22 D9 98 E6 1C 4A DC 06 ED DC B8 AC 23 11 22 12 FA 22 47 10 36 68 31 2D 61 2D AA
>>6D 00

<<00 A4 04 00 00
>>6F 10 84 08 A0 00 00 01 51 00 00 00 A5 04 9F 65 01 FF 90 00

<<80 50 00 00 08 12 EB FE 6D 3F 1C 05 E6 1C
>>00 00 31 15 27 04 48 20 65 68 01 02 02 28 8D 7D 77 3D 56 8C 7A D8 79 67 93 DA 2C 74 90 00

<<84 82 00 00 10 48 3D B6 4F 48 41 0F EE DF DB 1E 31 A6 90 64 08
>>90 00

<<80 E6 0C 00 20 07 45 47 59 48 43 57 57 08 45 47 59 48 43 57 57 00 08 45 47 59 48 43 57 57 00 01 00 02 C9 00 00
>>6F 00

Labels (1)
0 Kudos
1 Reply

487 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @chenchengbei ,

 

Which product are you working on? May I have the JCOP version info? Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos