blood pressure monitor portable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

blood pressure monitor portable

Jump to solution
2,404 Views
tinhnv92
Contributor I

Hi everyone, i am working with blood pressure monitor portable ,

I had finished analog circuit from sensor MPX5050 , then i want to test this circuit , but i don't have no idea , how to generate a blood pressure signal ! ,

can you help me ! Thanks  ,

here is my ciruits

0 Kudos
Reply
1 Solution
1,803 Views
Joshevelle
Senior Contributor I

Hello a b,

You’d need a blood pressure cuff. The pressure sensor would measure the pressure change in the cuff:

http://flightphysical.com/images/bodyparts/blood-pressure-cuff.jpg

In the above image you can see a blood pressure cuff with a mechanical pressure gauge, instead of that you would connect P1 of the MPX5050.

Please take a look at “Ankle-Brachial Index” image in the following page for detailed information on using a blood pressure cuff:

http://www.ehow.com/how_4425292_use-blood-pressure-cuff.html

If you’re only simulating the circuit, you’d need to generate a signal like the one shown in the following page:

http://www.biopac.ca/Continuous%20Non%20Invasive%20Blood%20Pressure.htm

I’d recommend you to run some test in Matlab or Octave, you can generate such signal by adding sinusoidal signals of different frequencies.

You could also download an artificial biomedical signal generator from the following page from OhioLINK ETD Center:

http://etd.ohiolink.edu/view.cgi/Bhojwani%20Soniya%20Naresh.pdf?akron1193079604

Hope it helps!

Josh

View solution in original post

0 Kudos
Reply
2 Replies
1,804 Views
Joshevelle
Senior Contributor I

Hello a b,

You’d need a blood pressure cuff. The pressure sensor would measure the pressure change in the cuff:

http://flightphysical.com/images/bodyparts/blood-pressure-cuff.jpg

In the above image you can see a blood pressure cuff with a mechanical pressure gauge, instead of that you would connect P1 of the MPX5050.

Please take a look at “Ankle-Brachial Index” image in the following page for detailed information on using a blood pressure cuff:

http://www.ehow.com/how_4425292_use-blood-pressure-cuff.html

If you’re only simulating the circuit, you’d need to generate a signal like the one shown in the following page:

http://www.biopac.ca/Continuous%20Non%20Invasive%20Blood%20Pressure.htm

I’d recommend you to run some test in Matlab or Octave, you can generate such signal by adding sinusoidal signals of different frequencies.

You could also download an artificial biomedical signal generator from the following page from OhioLINK ETD Center:

http://etd.ohiolink.edu/view.cgi/Bhojwani%20Soniya%20Naresh.pdf?akron1193079604

Hope it helps!

Josh

0 Kudos
Reply
1,803 Views
tinhnv92
Contributor I

sorry ; i just want to test in software !

0 Kudos
Reply