SENSOR SELECTION MPXV5010

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SENSOR SELECTION MPXV5010

跳至解决方案
445 次查看
kumod
Contributor II

IN MPXV5010 IF P1 > P2 OUTPUT GOES FROM 0.2 TO 5VOLT , I NEED SENSOR EXACT OPPOSITE WITH SAME RATING MEANS P1< P2 THEN OUT GOES 0.2 TO 4.5VOLT IS IT POOSIBLE OR SUGGEST PACKAGE OF THE MPXV5010G6U WHICH WILL HAVE ACCES TO USE THE p2 PORT FOR VACCUME INPUT , please suggest sensor with have vacuume pressure port is with port attched 

标记 (1)
0 项奖励
回复
1 解答
408 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
400 次查看
kumod
Contributor II

thanks

0 项奖励
回复
406 次查看
kumod
Contributor II

exact o to -10kpa is available or not

0 项奖励
回复
403 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

Exact to -10 kPa is not available.

BR, Tomas

0 项奖励
回复
409 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

0 项奖励
回复