SENSOR SELECTION MPXV5010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SENSOR SELECTION MPXV5010

Jump to solution
291 Views
kumod
Contributor II

IN MPXV5010 IF P1 > P2 OUTPUT GOES FROM 0.2 TO 5VOLT , I NEED SENSOR EXACT OPPOSITE WITH SAME RATING MEANS P1< P2 THEN OUT GOES 0.2 TO 4.5VOLT IS IT POOSIBLE OR SUGGEST PACKAGE OF THE MPXV5010G6U WHICH WILL HAVE ACCES TO USE THE p2 PORT FOR VACCUME INPUT , please suggest sensor with have vacuume pressure port is with port attched 

Tags (1)
0 Kudos
1 Solution
254 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

View solution in original post

0 Kudos
4 Replies
246 Views
kumod
Contributor II

thanks

0 Kudos
252 Views
kumod
Contributor II

exact o to -10kpa is available or not

0 Kudos
249 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

Exact to -10 kPa is not available.

BR, Tomas

0 Kudos
255 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

0 Kudos