SENSOR SELECTION MPXV5010

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SENSOR SELECTION MPXV5010

ソリューションへジャンプ
456件の閲覧回数
kumod
Contributor II

IN MPXV5010 IF P1 > P2 OUTPUT GOES FROM 0.2 TO 5VOLT , I NEED SENSOR EXACT OPPOSITE WITH SAME RATING MEANS P1< P2 THEN OUT GOES 0.2 TO 4.5VOLT IS IT POOSIBLE OR SUGGEST PACKAGE OF THE MPXV5010G6U WHICH WILL HAVE ACCES TO USE THE p2 PORT FOR VACCUME INPUT , please suggest sensor with have vacuume pressure port is with port attched 

タグ(1)
0 件の賞賛
返信
1 解決策
419件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
411件の閲覧回数
kumod
Contributor II

thanks

0 件の賞賛
返信
417件の閲覧回数
kumod
Contributor II

exact o to -10kpa is available or not

0 件の賞賛
返信
414件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

Exact to -10 kPa is not available.

BR, Tomas

0 件の賞賛
返信
420件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

0 件の賞賛
返信