IN MPXV5010 IF P1 > P2 OUTPUT GOES FROM 0.2 TO 5VOLT , I NEED SENSOR EXACT OPPOSITE WITH SAME RATING MEANS P1< P2 THEN OUT GOES 0.2 TO 4.5VOLT IS IT POOSIBLE OR SUGGEST PACKAGE OF THE MPXV5010G6U WHICH WILL HAVE ACCES TO USE THE p2 PORT FOR VACCUME INPUT , please suggest sensor with have vacuume pressure port is with port attched
Solved! Go to Solution.
Hello Kumod,
We can offer the following vacuum pressure sensors:
https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA
The closest one would be either the MPXV7007DP or MPXV7025DP.
BR, Tomas
thanks
exact o to -10kpa is available or not
Hello Kumod,
Exact to -10 kPa is not available.
BR, Tomas
Hello Kumod,
We can offer the following vacuum pressure sensors:
https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA
The closest one would be either the MPXV7007DP or MPXV7025DP.
BR, Tomas