Pressure Sensor: MPX4250 - Question about package size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pressure Sensor: MPX4250 - Question about package size

963件の閲覧回数
thomas81
Contributor I

Hi,

Is MPX4250 Series Pressure sensor (0 to 250 kPa, 0.2 to 4.9 V Output) available in a case size 482A-01?

The case size I need is same as MPXA4250AC6U:

However this series has a range of 20~250kPA. Looking for 0~250kPa.

Thanks

Tom

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

655件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Thomas,

Unfortunately not, the MPX4250 series of differential or gauge pressure sensors is only available in a Unibody package as shown in the device data sheet.

If you have any other questions, please let me know.

Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛