Measuring water level in the tank

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Measuring water level in the tank

2,424件の閲覧回数
PA3040
Contributor I

Dear All

Please advice me what is the most suitable sensor to measure water level and put the result in the LCD display

Water tank 500L

fixed on root top 6M

I would like to connect the sensor height from the ground about 2M

My Tank height 1M

width 1M

Pipe diameter 1.25cm ( hose connected to tank )

Please advice

Thanks in advance

0 件の賞賛
返信
1 返信

714件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The following application notes might help you to select a suitable device.


AN1950: Water Level Monitoring

http://www.freescale.com/files/sensors/doc/app_note/AN1950.pdf

AN1516: Liquid Level Control Using a Pressure Sensor

http://www.freescale.com/files/sensors/doc/app_note/AN1516.pdf


Regards,

Tomas